AXIS#.MOTOR.IPEAK

Description

This parameter configures the drive for the motor's peak, instantaneous-rated current. AXIS#.MOTOR.IPEAK is used to limit the magnitude of the torqueClosedTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist producing q-component current command (AXIS#.IL.CMD ).


  • This parameter is automatically configured for Kollmorgen motors when MOTOR.AUTOSET=1.

  • This parameter is required to be configured for all motor types.

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

mA

Range

0.200 to 1,000

Default Value

2

Data Type

Float

See Also

AXIS#.IL.LIMITP , AXIS#.IL.LIMITN

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.MOTOR.IPEAK 0x500B 0x12 UDINT 1000:1 - RW False
AXIS2.MOTOR.IPEAK 0x510B 0x12 UDINT 1000:1 - RW False